System Requirements

 

System Requirements

General

Ensure that your system complies with the necessary requirements before installation.

PC System

Minimum requirements:

oWindows 2000 / XP or Windows 7

oPentium PC (300 MHz or faster recommended)

oTCP/IP power supply (10 Mbps)

o64MB RAM (128MB recommended)

oFree hard-disk memory > 100 MB

oSuper VGA monitor (with a resolution of at least 800x600)

oCD-ROM drive

System Requirements

Version 1.0.3.0 of the library functions only with the corresponding firmware versions of PacDrive LXM62, LXM52 or ILM62 and the corresponding firmware version of the PacDrive Controller and the EcoStruxure Machine Expert.

The following table summarizes the system requirements for AutoTune:

Library

Drive (LXM62, LXM52, ILM62)

PacDrive Controller

EcoStruxure Machine Expert

AutoTune 1.1..x.0

V01.36.09.00 or higher

V01.36.01.00 or higher

V01.36.01.00 or higher

AutoTune 1.2.x.0

V01.50.04.00 or higher

V01.50.01.00 or higher

V01.50.01.00 or higher

AutoTune 1.3.x.0

V01.51.07.00 or higher

V01.51.01.00 or higher

V01.51.01.00 or higher

At least one drive of the type LXM62, LXM62Linear, LXM52, LXM52Linear or ILM62 is required.

Recommended configuration:

oFlashDisk with 16MB RAM in the PacDrive Controller.

Motion Axis Requirements

oThe axis must have an unrestricted range of motion.

oChanging moments of inertia J(ϕ) cannot be optimized

oMinimum range of motion, minimum speed, and minimum acceleration required