IF_RobotFeedbackSpace

 

IF_RobotFeedbackSpace - General Information

Overview

Type:

Interface

Available as of:

V1.0.0.0

Inherits from:

-

This chapter provides information on:

oTask

oDescription

oProperties

Task

Interface with return values of the robot motion in the Cartesian space.

Description

This interface is part of IF_RobotFeedback and contains data on the motion of the robot in the Cartesian space.

Properties

Name

Data type

Accessing

Description

ifX

IF_RobotFeedbackMotionCartesian

Read

Interface with return values for the motion of the TCP (Tool Center Point) along the X axis of the Cartesian coordinate system.

ifY

IF_RobotFeedbackMotionCartesian

Read

Interface with return values for the motion of the TCP along the Y axis of the Cartesian coordinate system.

ifZ

IF_RobotFeedbackMotionCartesian

Read

Interface with return values for the motion of the TCP along the Z axis of the Cartesian coordinate system.

lrCurvature

LREAL

Read

Curvature of the space movement.

oIF_RobotFeedback.ifSpace.lrCurvature; approximation of the curvature of the space movement considering a tracking movement.

oIF_RobotFeedback.ifTrajectoryStorage.ifSpace.lrCurvature; curvature of the space movement without considering a tracking movement. Only the movement caused by move commands is considered.

lrRefAccelerationRadial

LREAL

Read

Radial acceleration in the Cartesian space.

SQRT(AccResultant² + AccTangential²) 

lrRefAccelerationResultant

LREAL

Read

Resulting acceleration in the Cartesian space.

SQRT(AccX² + AccY² + AccZ²)

lrRefAccelerationTangential

LREAL

Read

Tangential acceleration in the Cartesian space.

lrRefVelocityTangential

LREAL

Read

Tangential velocity in the Cartesian space.

lrTrackingDeviation

LREAL

Read

Resulting tracking error in the Cartesian space.

SQRT(TDX² + TDY² + TDZ²)

rstTangent

REFERENCE TO PDL.ST_Vector3D

Read

Tangent of the Cartesian position along the connected path (refer to Behavior of rstTangent (tangent vector feedback).

rstEstimatedStopPosition

REFERENCE TO PDL.ST_Vector3D

Read

Estimated Cartesian stop position on the connected path including a potential tracking (refer to Behavior of feedback property rstEstimatedStopPosition).

xTrackingDeviationWarning

BOOL

Read

TRUE = The parameterized maximum tracking error along the path is exceeded.

FALSE = The parameterized maximum tracking error along the path is not exceeded.