ST_TrackingParameters - General Information
|
Type: |
Data structure |
|
Available as of: |
V2.14.0.0 |
|
Inherits from: |
- |
Structure to describe additional parameters for a tracking system.
Also refer to Minimizing the Influence of a Tracking System on the Trajectory of a Robot.
|
Variable |
Data type |
Description |
|---|---|---|
|
lrAccelerationZeroThreshold |
LREAL |
This value defines an acceleration limit for a tracking system. For accelerations below this limit, the state of the tracking system is treated as constant velocity or standstill during desynchronization phase. Valid values are: olrAccelerationZeroThreshold ≥ 0.0 olrAccelerationZeroThreshold = -1.0 To disable the detection of standstill or constant velocity set the value to -1.0. NOTE: Modifying the value for a tracking system via the method SetTrackingParameters() while the tracking system is active during the call of the method, is only taken into account after leaving and reentering the tracking system. |