Configuration of the Profinet IO Slave

 

Configuration of the Profinet IO Slave

Prerequisites

To use the Profinet IO Slave, you have to install the appropriate device description (Menu bar > Tools > Device Repository).

The Profinet XML-file (GSDML-V2.33-Schneider Electric-PacDrive-20170725.xml) is located at: C:\Users\Public\Public Documents\SoMachine Software\Vx.xx Motion\Documents\FieldbusDescriptionFiles.

Refer to Online Help: Online Help Overview and Menu Commands\Tools Menu Commands\Repository-Related Commands\Device Repository....

Add Profinet IO Master to PLC Configuration

Step

Action

1

Open your project in the Logic Builder.

2

Select the PacDrive controller.

3

Right-click > Add Device.

Result: The Add Device dialog is displayed.

4

Select Fieldbusses > Profinet IO  > Profinet IO Master > PROFINETIO-Controller (Schneider Electric).

5

Confirm with Add Device.

6

Close the dialog.

7

Double-click the PNC_Controller (PROFINETIO-Controller) in the Devices tree to open its device editor dialog.

8

In the NetX Configuration tab, select the appropriate Connector (for example Front / 1).

9

In the General tab set the appropriate IP Parameters.

Add Profinet IO Slave to PLC Configuration

Step

Action

1

Select the PNC_Controller (PROFINETIO-Controller).

2

Right-click > Add Device.

Result: The Add Device dialog is displayed.

3

Select Fieldbusses > Profinet IO > Profinet IO Slave > Schneider_Electric_PN Device.

4

Confirm with Add Device.

5

Close the dialog.

Scan For Devices and Enter Station Name and IP Address

Step

Action

1

Download your project.

2

Login.

3

Select the PNC_Controller (PROFINETIO-Controller).

4

Right-click > Scan For Devices.

5

Copy Station Name and IP Address of the Schneider_Electric_PN Device to the scanned device.

G-SE-0068373.1.png

 

 

6

Confirm Station Name and IP Address by clicking Set Name+IP.

7

Click Scan Devices to rescan the Profinet network.

Now the following parameters are displayed for the Scanned Device:

oDevicename

oDevicetype

oStation Name

oIdent-No.

oMAC address

oIP address

oSubnet mask