StopBits

 

StopBits

General

Type

EF

Devices supporting the parameter

COM

Traceable

Yes

Functional Description

Selects the number of stop bits

Value

Data type

Meaning

1 Bit / 0

DINT

1 stop bit

2 Bits / 1

DINT

2 sop bits