STO - Safe Torque Off function

 

General function description

The STO function is the most common and basic drive integrated safety-related function. If STO is activated, no more power, which can cause rotation or motion, is applied to the motor. The power stage of the drive will not provide any energy to the motor which can generate torque or force in case of a linear motor.

An active STO function results in a subsequent start-up/restart inhibit (see section below).

The STO function prevents an unintended start according to the stan­dard EN 60204-1, section 5.4. With the designated STO function acti­vated, the power stage of the drive is deactivated. The drive is then torque-free. This state is monitored internally in the drive.

Requesting/monitoring by the safety-related FB/Safety Module

Immediately with the STO activation the drive is set torque-free and the axis then coasts down until speed is zero.

SafeTorqueOff.png

When requesting STO, the safety-related function is executed immedi­ately. STO can be requested by switching the signal at input S_STO_Request to SAFEFALSE (if input Activate = TRUE) or via the hard-wired link (if Safety Module device parameter HW_STO = Activated). Refer to the section below.

The torque-free status of the drive is indicated by switching the function block output S_STO_SafetyActive to SAFETRUE.

After indicating the active STO function, the axis coasts down. There­fore, S_STO_SafetyActive = SAFETRUE does not necessarily imply the standstill of the axis. The coast down time depends on physical proper­ties of the used components, such as weight, torque, friction, etc.

WARNING

UNINTENDED EQUIPMENT OPERATION

  • Make certain that no hazards can arise for persons or material during the coast down period of the axis/machine.

  • Do not enter the zone of operation during the coast down period.

  • Ensure that no other persons can access the zone of operation during the coast down period.

  • Use appropriate safety interlocks where personnel and/or equip­ment hazards exist.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

Application

As the STO function of the drive disables the power stage to the motor, it is suitable to be used in applications where the axis comes to a stop by itself in a sufficiently short time through its load torque or friction or when the "coast down" of the axis has no safety-related relevance.

STO as general functional safe state: The STO function is defined as the default functional safe state. Therefore, the STO function is the final fallback function of the other safety-related functions described in this documentation.

STO request via the function block or hard-wired

Depending on your requirements and the implementation of the system, the STO function can be requested in two ways:

Further Information

Refer to the topic "STO hard-wired" for detailed information.

Start-up inhibit: STO following the function block activation

After its start-up the Safety Module automatically enters the STO func­tionally-safe state. According to the relevant IEC 60204-1 standard, the STO function executes stop category 0. This stop category implies a subsequent start-up inhibit. The start-up inhibit is only removed if there is a positive signal edge at the Reset input of the safety-related function block.

Restart inhibit following an STO

After removing an STO function request by switching the respective function block input from SAFEFALSE to SAFETRUE, a restart inhibit is automatically activated to prevent the unintended restart of the axis. According to the relevant IEC 60204-1 standard, the STO function executes stop category 0. This stop category implies a subsequent restart inhibit. The restart inhibit is only removed if there is a positive signal edge at the Reset input of the safety-related function block.

Relevant Safety Module device parameters

How to edit the relevant safety-related device parameters: In the EcoStruxure Machine Expert - Safety 'Devices' window, ...

  1. Left-click the Safety Module in the devices tree.

  2. In the Device Parameterization editor on the right, scroll to the rele­vant parameter section (see table heading below).

  3. Specify the parameters listed in the table below for this safety-related function.

For detailed information on the value range and default value for the parameter, refer to the corresponding chapter for the safety module used in the "Safety Module Parameters and Process Data Items" guide.

Parameter section: Basic

HW_STO

  • Activated

    The hard-wired signal link can also be used. The STO function can be requested via the function block (S_STO_Request input = SAFEFALSE) as well as via the direct hard-wired signal link on the drive.

  • Deactivated

    The hard-wired signal link cannot be used. The STO function can solely be requested via the function block (S_STO_Request input = SAFEFALSE).

WARNING

NON-CONFORMANCE TO SAFETY FUNCTION REQUIRE­MENTS

  • Verify that the device parameters for the Safety Module correspond to your risk analysis.

  • Be sure that your risk analysis includes an evaluation for setting incorrectly device parameter values.

  • Validate the overall safety-related function with regard to the set device parameter values and thoroughly test the application.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

Relevant FB inputs/outputs and bits in status word