Abbreviation |
In full |
Standard |
ESPE |
Electro-Sensitive Protective Equipment |
IEC 61496-1 |
EDM |
External Device Monitoring Safety-related function block for monitoring the initial state and the switching behavior of contactors connected to the Safety Logic Controller (external contactor monitoring). |
-/- |
Cat. |
Category Basis for determining the performance level (» PL) of a safety-related controller. |
EN ISO 13849-1 |
OSSD |
Output Signal Switching Device Part of the ESPE, which can be connected to the machine control system and switched off via a request for the safety-related function. |
-/- |
PL |
Performance Level Value for the average probability of dangerous failure of safety-related machine control systems. The category (Cat.) and the probability-related properties of the components used form the basis for determining the PL. The target PL results in binding, safety-related design principles, which aim to minimize the risk of a malfunction. |
EN ISO 13849-1 |
SIL |
Safety Integrity Level Value for assessing electrical/electronic/programmable electronic systems in terms of the reliability of their safety-related functions. The target SIL results in binding, safety-related design principles, which aim to minimize the risk of a malfunction. |
IEC 61508 |
SILCL |
SIL Claim Limit, maximum SIL value for a subsystem. |
EN 62061 |