About the Magelis SCU HMI Controller
Magelis SCU HMI Controller Devices Overview
The Schneider Electric Magelis SCU HMI Controller has various powerful features. This controller can service a wide range of applications.
The software configuration and programming is accomplished with the SoMachine software.
The Magelis SCU HMI Controller is supported and programmed with the SoMachine software, which supports the following IEC61131-3 programming languages:
oIL: Instruction List
oST: Structured Text
oFBD: Function Block Diagram
oSFC: Sequential Function Chart
oLD: Ladder Diagram
SoMachine software can also be used to program these controllers using CFC (Continuous Function Chart) language.
The Magelis SCU HMI Controller includes a Real Time Clock (RTC) system.
The Magelis SCU HMI Controller can be operated externally by the following:
oa Run/Stop operation by a dedicated digital input, defined in the software configuration. For more information, refer to Configuration of Digital Inputs.
oa SoMachine software command.
The table shows the memory specifications:
|
Area |
Element |
Size (bytes) |
|---|---|---|
|
System Area |
System area reserved memory |
131072 |
|
System and diagnostic variables |
||
|
Physical input addresses (%I) |
256 |
|
|
Physical output addresses (%Q) |
256 |
|
|
Retain variables (1) |
16360 |
|
|
Persistent retain variables |
2044 |
|
|
Application Area |
Compiled control application |
1024000 |
|
User Area |
Symbols |
Dynamic allocation of 1024000 |
|
Variables |
||
|
Libraries |
||
|
(1) Not all of the 16360 bytes are available for the customer application because some libraries may use retain variables. |
||
The following embedded I/O types are available, depending on the controller model:
oRegular inputs
oFast inputs (HSC)
oRegular outputs
oFast outputs (PTO/PWM)
oAnalog outputs
oThermocouple inputs
oRTD (Resistance Temperature Detector) inputs
Embedded Communication Features
4 types of communication ports are available on the rear panel:
oEthernet port
oCANopen
oUSB programming ports
oSerial link port
For more details, refer to the chapter Integrated Communication Ports.
Magelis SCU HMI Controller Range
|
Reference |
Digital Input |
Digital Output |
Analog Input |
Analog Output |
Screen Size |
|---|---|---|---|---|---|
|
HMISCU6A5 |
14 regular inputs and 2 fast inputs (HSC)(1) |
8 regular outputs and 2 fast outputs (PTO)(2) |
No |
No |
8.9 cm (3.5 in.) |
|
HMISCU8A5 |
14.48 cm (5.7 in.) |
||||
|
HMISAC |
No |
||||
|
HMISCU6B5 |
6 regular inputs and 2 fast inputs (HSC)(1) |
6 regular outputs and 2 fast outputs (PTO)(2) |
2 analog inputs (12-bit plus sign SAR ADC) and 2 analog inputs (16-bit), thermocouple, and RTD |
2 analog outputs (12-bit) |
8.9 cm (3.5 in.) |
|
HMISCU8B5 |
14.48 cm (5.7 in.) |
||||
|
HMI SBC |
No |
||||
|
(1) The fast inputs can be used either as regular inputs or as fast inputs for counting or event functions. (2) The fast outputs can be used either as regular outputs or as fast outputs for PTO, PWM functions, or reflex output for HSC. |
|||||