Additional application example

This section describes an additional possible application, where the function block evaluates a three-stage enable switch.

The function block must only be used in an actual application once a risk analysis has been conducted.

Details of the risk category/SIL/PL have not been included here, as clas­sification is always based on the application in which the function block is used.

NOTE:

The use of the function block alone is not sufficient to execute the safety-related function according to the Cat./SIL/PL deter­mined by the risk analysis. In conjunction with the safety-related I/O device used, additional measures must be taken to meet the requirements of the safety-related function. These include, for example, the appropriate wiring and parameterization of the inputs and outputs as well as measures to exclude (design out) errors that cannot be detected. For additional information, refer to the documentation provided with the safety-related I/O device used.

NOTE:

Refer to the notes in the User Manual on proper electrical connec­tion of the Safety Logic Controller and the extension modules (e.g., connecting the three-stage, manually actu­ated enable switch).

Evaluating a three-stage enable switch. Confirming the selected operating mode using SF_ModeSelector.

This example describes the evaluation of a three-stage enable switch by the SF_EnableSwitch function block. The enable switch is used to manually confirm an operating mode of a machine. The operating mode is selected by means of a three-stage mode selector switch S1, which is evaluated using the safety-related SF_ModeSelector function block.

In order to operate the controlled machine in operating mode 2 (in the example shown, this is setup mode) or 3 (manual mode), the selected mode must be enabled manually by pressing the enable switch.

Connecting the SF_EnableSwitch function block:

Connecting the SF_ModeSelector function block:

NOTE:

Notes on the graphic:

The S_Mode0Sel to S_Mode2Sel enable signals of the SF_ModeSe­lector function block have the following functions:

(1): Automatic mode.

(2): Setup mode. Request for the safely reduced speed at the speed monitor.

(3): Manual mode.

Connecting the SF_EnableSwitch function block:

(4): The S_SafetyActive input of the SF_EnableSwitch function block is connected to the feedback signal of the speed monitor. This feedback signal is used to set the operating mode selected (reduced speed).

(5): The S_EnableSwitchOut enable signal of the SF_EnableSwitch function block is connected to additional safety-related function blocks or functions and controls the application accordingly.

PROG_EnableSwitch_ApplicationExample2.png

S1

Mode selector switch with 3 switch positions

S2

Key switch

S3

Confirmation

S4

Reset

S5

Three-stage enable switch

noteOnImage.png 

See note above the illustration.