EcoStruxure Machine Expert version 1.1 does not support the M258, LMC058 and LMC078 controllers.

Log File

 

Log File

Overview

EcoStruxure Machine Expert automatically creates a log file. It provides information that is useful for debugging purposes. The size of the file is not restricted and there is no automatic removal or overwriting procedure.

The file is deleted only when EcoStruxure Machine Expert is uninstalled.

NOTE: Delete the file manually in suitable time intervals so that it does not use a large amount of disk space on your PC. The file is found in the temporary folder of Windows, defined by the variable %TEMP%.