EcoStruxure Machine Expert version 1.1 does not support the M258, LMC058 and LMC078 controllers.

Global Variables List (GVL) Editor

 

GVL Editor

Overview

The GVL editor is a Declaration Editor for editing Global Variables Lists. The GVL editor works as does the Declaration Editor and corresponds to the options, both offine and online, set for the text editor. The declaration starts with VAR_GLOBAL and ends with END_VAR. These keywords are provided automatically. Enter valid declarations of global variables between them.

GVL editor

G-SE-0025793.1.gif-high.gif

 

 

GVL Editor Used as Persistent Variables Editor

The GVL editor can also be used to manage Persistent Variables objects. In this case, the editor contains declarations of VAR_GLOBAL PERSISTENT variables. For further information, refer to the chapter Persistent Variables .