SysDirCopy (FUN)

 

FUNCTION SysDirCopy : RTS_IEC_RESULT

Copies the contents of szSourceDir to szDestDir. Depending of the parameters, all subdirectories and its content will be copied too, and existing files will be overwritten. NOTE: Empty direcories will be copied if xRecursive is TRUE.

InOut:

Scope

Name

Type

Comment

Return

SysDirCopy

RTS_IEC_RESULT

Returns the runtime system error code (see CmpErrors_Itf.library)

Input

szDestDir

REFERENCE TO STRING

Name of destination directory

szSourceDir

REFERENCE TO STRING

Name of source directory

xRecursive

BOOL

TRUE: all subdirectories and their contents are copied, FALSE: subdirectories are omitted

xOverwrite

BOOL

TRUE: existing files are overwritten, FALSE: existing files are left untouched