FUNCTION SysDirGetCurrent : RTS_IEC_RESULT
Get current working directory for IEC file access
InOut:
Scope |
Name |
Type |
Comment |
Return |
SysDirGetCurrent |
RTS_IEC_RESULT |
Returns the runtime system error code (see CmpErrors_Itf.library) |
Input |
szDir |
REFERENCE TO STRING |
OUT_PARAMETER: Name of current directory |
diMaxDirLen |
DINT |
Max lenght of directory buffer |