FUNCTION SysDirRead : RTS_IEC_RESULT
Read next directory entry. Writes the entry in pszDirEntry.
InOut:
|
Scope |
Name |
Type |
Comment |
|
Return |
SysDirRead |
RTS_IEC_RESULT |
Returns the runtime system error code (see CmpErrors.library)
Note Typically after error ERR_BUFFERSIZE, the dir-handle is set to the next entry, so this entry will be missed! |
|
Input |
hDir |
RTS_IEC_HANDLE |
Handle to directory opened with SysDirOpen |
|
szDirEntry |
REFERENCE TO STRING |
OUT_PARAMETER: Directory entry as string |
|
|
diMaxDirEntry |
DINT |
OUT_PARAMETER: Max number of bytes to write in pszDirEntry |
|
|
pDirInfo |
POINTER TO DirInfo |
OUT_PARAMETER: Directory information NOTE: Can be 0 (so only directory name is provided in pszDirEntry) |