FUNCTION SysFileCopy : RTS_IEC_RESULT
Copy one file to another.
A standard path will be added to the filename, if no path is specified.
InOut:
|
Scope |
Name |
Type |
Comment |
|
Return |
SysFileCopy |
RTS_IEC_RESULT |
The runtime system error code (see CmpErrors.library) |
|
Input |
szDestFileName |
STRING |
Destination file name. File name can contain an absolute or relative path to the file. Path entries must be separated with a Slash (/) and not with a Backslash (\)! |
|
szSourceFileName |
STRING |
Source file name. File name can contain an absolute or relative path to the file. Path entries must be separated with a Slash (/) and not with a Backslash (\)! |
|
|
pulCopied |
POINTER TO __XWORD |
Number of bytes copied |