SysFileDeleteByHandle (FUN)

 

FUNCTION SysFileDeleteByHandle : RTS_IEC_RESULT

Delete the file specified by handle

InOut:

Scope

Name

Type

Comment

Return

SysFileDeleteByHandle

RTS_IEC_RESULT

Returns the runtime system error code (see CmpErrors.library)

Input

hFile

RTS_IEC_HANDLE

Handle of the file