FUNCTION SysFileFlush : RTS_IEC_RESULT
Flush the file cache and write into the file
InOut:
|
Scope |
Name |
Type |
Comment |
|
Return |
SysFileFlush |
RTS_IEC_RESULT |
Returns the runtime system error code (see CmpErrors_Itfs.library):
|
|
Input |
hFile |
RTS_IEC_HANDLE |
Handle of the file |