FUNCTION SysFileGetSize : __XWORD
Get file size of the file specified by name.
A standard path will be added to the filename, if no path is specified.
InOut:
|
Scope |
Name |
Type |
Comment |
|
Return |
SysFileGetSize |
__XWORD |
Size of the file in bytes |
|
Input |
szFileName |
STRING |
File name. File name can contain an absolute or relative path to the file. Path entries must be separated with a Slash (/) and not with a Backslash (\)! |
|
pResult |
POINTER TO RTS_IEC_RESULT |
Pointer to runtime system error code (see CmpErrors.library):
|