FUNCTION SysFileGetSizeByHandle : __XWORD
Get file size of the file specified by handle
InOut:
Scope |
Name |
Type |
Comment |
Return |
SysFileGetSizeByHandle |
__XWORD |
Size of the file in bytes |
Input |
hFile |
RTS_IEC_HANDLE |
Handle of the file |
pResult |
POINTER TO RTS_IEC_RESULT |
Pointer to runtime system error code (see CmpErrors.library) |