FUNCTION SysFileGetTime : RTS_IEC_RESULT
Get file time of the specified file.
A standard path will be added to the filename, if no path is specified.
InOut:
Scope |
Name |
Type |
Comment |
Return |
SysFileGetTime |
RTS_IEC_RESULT |
The runtime system error code (see CmpErrors.library) |
Input |
szFileName |
STRING |
File name. File name can contain an absolute or relative path to the file. Path entries must be separated with a Slash (/) and not with a Backslash (\)! |
ptFileTime |
POINTER TO SYS_FILETIME |
Pointer to get the file time results. |