FUNCTION SysFileRead : __XWORD
Read number of bytes out of the file
InOut:
Scope |
Name |
Type |
Comment |
Return |
SysFileRead |
__XWORD |
Number of bytes read from file. 0=if failed |
Input |
hFile |
RTS_IEC_HANDLE |
Handle of the file |
pbyBuffer |
POINTER TO BYTE |
Pointer to buffer for read data |
|
ulSize |
__XWORD |
Number of bytes to read from file. Must be less or equal the buffer size! |
|
pResult |
POINTER TO RTS_IEC_RESULT |
Pointer to runtime system error code (see CmpErrors.library) |