FUNCTION SysFileRename : RTS_IEC_RESULT
Rename the file.
A standard path will be added to the filename, if no path is specified.
InOut:
|
Scope |
Name |
Type |
Comment |
|
Return |
SysFileRename |
RTS_IEC_RESULT |
Returns the runtime system error code (see CmpErrors.library) |
|
Input |
szOldFileName |
STRING |
Old file name. File name can contain an absolute or relative path to the file. Path entries must be separated with a Slash (/) and not with a Backslash (\)! |
|
szNewFileName |
STRING |
New file name. File name can contain an absolute or relative path to the file. Path entries must be separated with a Slash (/) and not with a Backslash (\)! |