FUNCTION SysFileSetPos : RTS_IEC_RESULT
Set the file pointer to the specified position
InOut:
Scope |
Name |
Type |
Comment |
Return |
SysFileSetPos |
RTS_IEC_RESULT |
Returns the runtime system error code (see CmpErrors.library) |
Input |
hFile |
RTS_IEC_HANDLE |
Handle of the file |
ulOffset |
__XWORD |
Offset to set from the beginning of the file |