FUNCTION SysFileTruncate : RTS_IEC_RESULT
Set a new filesize. May be larger or smaller than current size.
InOut:
Scope |
Name |
Type |
Comment |
Return |
SysFileTruncate |
RTS_IEC_RESULT |
Returns the runtime system error code (see CmpErrors.library) |
Input |
hFile |
RTS_IEC_HANDLE |
Handle of the file |
ulSizeNew |
__XWORD |
Size to set. |