FUNCTION SysFileWrite : __XWORD
Write number of bytes to the file. File must be opened with AM_WRITE or AM_APPEND.
InOut:
Scope |
Name |
Type |
Comment |
Return |
SysFileWrite |
__XWORD |
Number of bytes written to the file. 0=if failed |
Input |
hFile |
RTS_IEC_HANDLE |
Handle of the file |
pbyBuffer |
POINTER TO BYTE |
Pointer to buffer with data to write to file |
|
ulSize |
__XWORD |
Number of bytes to write in the file. Must be less or equal the buffer size! |
|
pResult |
POINTER TO RTS_IEC_RESULT |
Pointer to runtime system error code (see CmpErrors.library) |