DWORD_AS_WORD: Splitting the Double Word into Two Words
This figure shows the pin diagram of the DWORD_AS_WORD function block:
The DWORD_AS_WORD function block converts an input value of data type DWORD to lower and higher outputs of type WORD.
The input double word i_dwIput is split into two words, higher q_wHigh and lower q_wLow words.
This table describes the input pins of the DWORD_AS_WORD function block:
|
Input |
Data Type |
Description |
|---|---|---|
|
i_dwIput |
DWORD |
Input value Range: 0...4294967295 |
This table describes the output pins of the DWORD_AS_WORD function block:
|
Output |
Data Type |
Description |
|---|---|---|
|
q_wLow |
WORD |
Lower word output value Range: 0...65535 |
|
q_wHigh |
WORD |
Higher word output value Range: 0...65535 |