Frequency_TO_Period: Calculating Period of Time of Given Frequency
This figure shows the pin diagram of the Frequency_TO_Period function:
The Frequency_TO_Period function converts frequency (Hertz) value of type REAL to time. This result is of TIME type.
The period of time is calculated with the given frequency. The frequency is set in i_rIput pin in REAL data format. The equivalent time value is returned in Frequency_TO_Period pin in TIME data format.
Period = 1 / Frequency
NOTE: If the input is not in the previous range, the output is zero.
This table describes the input pins of the Frequency_TO_Period function:
|
Input |
Data Type |
Description |
|---|---|---|
|
i_rIput |
REAL |
Input Frequency 0.0...1000.0Hz |
This table describes the output pins of the Frequency_TO_Period function:
|
Output |
Data Type |
Description |
|---|---|---|
|
Frequency_TO_Period |
TIME |
Period of time of the frequency input. 0...4294967295 ms |