The global parameter list (GPL) contains global constants which are used by filtering function blocks of this library. The parameters can be edited individually for each application where the library is used. The modification must be done within the Library Manager of the project where the library is referenced.
Variable |
Data type |
Default value |
Range |
Description |
---|---|---|---|---|
Gc_uiMaxAvgeSmpl |
UINT |
100 |
100... 1000 |
The maximum number of samples counted by the i_uiSmplCnt input . |