Normalizer_With_Limiter: Scaling the Minimum and Maximum Input
Normalizer_With_Limiter Function Block
This figure shows the pin diagram of the Normalizer_With_Limiter function block:
The Normalizer_With_Limiter function block scales the minimum and maximum input value to the range of minimum and maximum output value. The input value can be limited to minimum and maximum output values.
The output value can be limited to minimum and maximum output values using i_xIputMinLim and i_xIputMaxLim.
When the input exceeds the maximum/minimum input limit value q_xIputLimExcd will be TRUE.
|
i_xIputMaxLim |
i_xIputMinLim |
i_rIput |
q_rOput |
q_xIputLimExcd |
|---|---|---|---|---|
|
FALSE |
FALSE |
12.5 |
3072 |
TRUE |
|
TRUE |
FALSE |
12.5 |
2048 |
TRUE |
|
TRUE |
FALSE |
10 |
2048 |
FALSE |
|
TRUE |
FALSE |
7.5 |
1024 |
FALSE |
|
TRUE |
TRUE |
5 |
0 |
FALSE |
|
FALSE |
TRUE |
2.5 |
-1024 |
FALSE |
|
FALSE |
TRUE |
0 |
-2048 |
FALSE |
|
FALSE |
TRUE |
-2.5 |
-2048 |
TRUE |
|
FALSE |
FALSE |
-2.5 |
-3072 |
TRUE |
This table describes the input pins of the Normalizer_With_Limiter function block:
|
Input |
Data Type |
Description |
|---|---|---|
|
i_rIput |
REAL |
Input value Range: ±3.4e+38 |
|
i_rIputMin |
REAL |
Minimum input Range: ±3.4e+38 |
|
i_rIputMax |
REAL |
Maximum input value Range: ±3.4e+38 |
|
i_rOputMin |
REAL |
Minimum output value Range: ±3.4e+38 |
|
i_rOputMax |
REAL |
Maximum output value Range: ±3.4e+38 |
|
i_xIputMinLim |
BOOL |
TRUE: Limit enabled for minimum input value FALSE:Limit disabled |
|
i_xIputMaxLim |
BOOL |
TRUE: Limit enabled for maximum input value FALSE:Limit disabled |
This table describes the output pins of the Normalizer_With_Limiter function block:
|
Output |
Data Type |
Description |
|---|---|---|
|
q_rOput |
REAL |
Scale output value Range: ±3.4e+38 |
|
q_xIputLimExcd |
BOOL |
Input value exceed limit value |