ONE_SEC_PULSE: Providing Pulses Every One Second
This figure shows the pin diagram of the ONE_SEC_PULSE function block:
The ONE_SEC_PULSE function block generates pulses of one second duration at the output q_xOput.
This table describes the output pins of the ONE_SEC_PULSE function block:
|
output |
Data Type |
Description |
|---|---|---|
|
q_xOput |
BOOL |
Output Pulse Output state = TRUE during 1 cycle of task Frequency = 1 Hz |
Instantiation and Usage Example
The above figure shows an instance of ONE_SEC_PULSE function block: