Period_TO_Frequency: Calculating Frequency of Given Time
This figure shows the pin diagram of the Period_TO_Frequency function:
The Period_TO_Frequency function converts time of type TIME to frequency(Hertz).This result is a REAL number.
This function calculates the frequency of given period of time. Time is set in i_rIput pin in TIME data format. The equivalent frequency value is returned in Period_TO_Frequency pin in REAL data format.
Frequency = 1 / Period
This table describes the input pins of the Period_TO_Frequency function:
|
Input |
Data Type |
Description |
|---|---|---|
|
i_tIput |
TIME |
Input time value Range: 0...4294967295 ms |
NOTE: If the input is not in the previous range, the output will be zero.
This table describes the output pins of the Period_TO_Frequency function:
|
Output |
Data Type |
Description |
|---|---|---|
|
Period_TO_Frequency |
REAL |
Equivalent frequency of the time input Range: 0...1000 Hz |