SetBitTo: Setting/Resetting One Bit
This figure shows the pin diagram of the SetBitTo function:
The SetBitTo function sets/resets (according to set) one bit specified by the bit in the given DWORD input. The bits are counted from low to high starting with 0.
The valid range is 0 to 31.
This table describes the input pins of the SetBitTo function:
|
Input |
Data Type |
Description |
|---|---|---|
|
i_dwIput |
DWORD |
Input value Range: 0...4294967295 |
|
i_iPos |
INT |
Bit position Range: 0...31 |
|
i_xSet |
BOOL |
TRUE: Set FALSE: Reset. |
This table describes the output pins of the SetBitTo function:
|
Output |
Data Type |
Description |
|---|---|---|
|
SetBitTo |
DWORD |
Output value Range: 0...4294967295 |
If the i_iPos input is not within the valid range, the input will be interpretated in modulo mode.