FUNCTION BCD_TO_INT : INT
Converts one byte in BCD format into an INT value
Example in ST:
i := BCD_TO_INT(73); (* Result is 49 *)
k := BCD_TO_INT(151); (* Result is 97 *)
l := BCD_TO_INT(15); (* Output -1, because it is not in BCD format *)
InOut:
|
Scope |
Name |
Type |
Comment |
|
Return |
BCD_TO_INT |
INT |
Value as INT for the input B |
|
Input |
B |
BYTE |
Value in BCD code. If the value is not in the BCD format, then the output is -1. |