BIT_AS_WORD (FB)

 

FUNCTION_BLOCK BIT_AS_WORD

Converts 16 input values of data type BOOL into an output value of the data type WORD

InOut:

Scope

Name

Type

Comment

Input

B00

BOOL

Input bit 0

B01

BOOL

Input bit 1

B02

BOOL

Input bit 2

B03

BOOL

Input bit 3

B04

BOOL

Input bit 4

B05

BOOL

Input bit 5

B06

BOOL

Input bit 6

B07

BOOL

Input bit 7

B08

BOOL

Input bit 8

B09

BOOL

Input bit 9

B10

BOOL

Input bit 10

B11

BOOL

Input bit 11

B12

BOOL

Input bit 12

B13

BOOL

Input bit 13

B14

BOOL

Input bit 14

B15

BOOL

Input bit 15

Output

W

WORD

Output value