BYTE_AS_BIT (FB)

 

FUNCTION_BLOCK BYTE_AS_BIT

Converts an input value of data type byte into 8 outputs of data type BOOL

InOut:

Scope

Name

Type

Comment

Input

B

BYTE

Input value

Output

B0

BOOL

Output bit 0

B1

BOOL

Output bit 1

B2

BOOL

Output bit 2

B3

BOOL

Output bit 3

B4

BOOL

Output bit 4

B5

BOOL

Output bit 5

B6

BOOL

Output bit 6

B7

BOOL

Output bit 7