DateTime (STRUCT)

 

TYPE DateTime : STRUCT

Two formats are supported:

Note

The following applies for the summer time in Europe: The switch to summer time is done on the last Sunday in March. At 2:00 a.m. the clock is set ahead by one hour. The following applies for the winter time (standard time) in Europe: The switch to winter time is done on the last Sunday in October. At 3:00 a.m. the clock is set back by one hour.

InOut:

Name

Type

Comment

uiYear

YEAR

uiMonth

MONTH

uiDay

DAY

If Year = 0, then 1..5 1 => first day in this month, 5 => last day in this month

uiHour

HOUR

uiMinute

MINUTE

uiSecond

SECOND

uiMilliseconds

MILLISECOND

eWeekday

WEEKDAY