FUNCTION_BLOCK DWORD_AS_BIT
Converts an input value of data type DWORD into 32 outputs of data type BOOL
InOut:
Scope |
Name |
Type |
Comment |
Input |
X |
DWORD |
Input value |
Output |
B00 |
BOOL |
Output bit 0 |
B01 |
BOOL |
Output bit 1 |
|
B02 |
BOOL |
Output bit 2 |
|
B03 |
BOOL |
Output bit 3 |
|
B04 |
BOOL |
Output bit 4 |
|
B05 |
BOOL |
Output bit 5 |
|
B06 |
BOOL |
Output bit 6 |
|
B07 |
BOOL |
Output bit 7 |
|
B08 |
BOOL |
Output bit 8 |
|
B09 |
BOOL |
Output bit 9 |
|
B10 |
BOOL |
Output bit 10 |
|
B11 |
BOOL |
Output bit 11 |
|
B12 |
BOOL |
Output bit 12 |
|
B13 |
BOOL |
Output bit 13 |
|
B14 |
BOOL |
Output bit 14 |
|
B15 |
BOOL |
Output bit 15 |
|
B16 |
BOOL |
Output bit 16 |
|
B17 |
BOOL |
Output bit 17 |
|
B18 |
BOOL |
Output bit 18 |
|
B19 |
BOOL |
Output bit 19 |
|
B20 |
BOOL |
Output bit 20 |
|
B21 |
BOOL |
Output bit 21 |
|
B22 |
BOOL |
Output bit 22 |
|
B23 |
BOOL |
Output bit 23 |
|
B24 |
BOOL |
Output bit 24 |
|
B25 |
BOOL |
Output bit 25 |
|
B26 |
BOOL |
Output bit 26 |
|
B27 |
BOOL |
Output bit 27 |
|
B28 |
BOOL |
Output bit 28 |
|
B29 |
BOOL |
Output bit 29 |
|
B30 |
BOOL |
Output bit 30 |
|
B31 |
BOOL |
Output bit 31 |