FUNCTION_BLOCK GEN
Generates periodic functions of different, given types
The generation may be done relative to a specific time base or a given call-count base (BASE). An example set of available types of periodic functions are shown in the following image.
InOut:
|
Scope |
Name |
Type |
Initial |
Comment |
|
Input |
MODE |
Types available:
|
||
|
BASE |
BOOL |
FALSE: Period referring to call ( CYCLES) TRUE: Period referring to time ( PERIOD) |
||
|
PERIOD |
TIME |
TIME#1s0ms |
Period time, only relevant if BASE = TRUE |
|
|
CYCLES |
INT |
1000 |
Number of calls per period, only relevant if BASE = FALSE |
|
|
AMPLITUDE |
INT |
Amplitud of the function to be generated |
||
|
RESET |
BOOL |
TRUE: Sets OUT to zero |
||
|
Output |
OUT |
INT |
Generated function value |