FUNCTION INT_TO_BCD : BYTE
Converts an INT value into a byte in BCD code
Example in ST:
i := INT_TO_BCD(49); (* Result is 73 *)
k := BCD_TO_INT(97); (* Result is 151 *)
l := BCD_TO_INT(100); (* Error! Output: 255 *)
InOut:
|
Scope |
Name |
Type |
Comment |
|
Return |
INT_TO_BCD |
BYTE |
Value in BCD code for the input I |
|
Input |
I |
INT |
Value as INT. A wrong value (<0 or >99) causes a return of 255. |