PACK (FUN)
FUNCTION PACK : BYTE
Packs 8 bits into 1 byte
InOut:
Scope
Name
Type
Comment
Return
PACK
BYTE
Value for the input BO..B7
Input
B0
BOOL
Input bit 0
B1
Input bit 1
B2
Input bit 2
B3
Input bit 3
B4
Input bit 4
B5
Input bit 5
B6
Input bit 6
B7
Input bit 7