PUTBIT (FUN)

 

FUNCTION PUTBIT : DWORD

Sets a bit of a DWORD value

Example in ST:

var1 := 38;   (* binär 100110 *)
var2 := PUTBIT(A,4,TRUE); (* Result: 54 = 2#110110 *)
var3 := PUTBIT(A,1,FALSE); (* Result: 36 = 2#100100 *)

InOut:

Scope

Name

Type

Comment

Return

PUTBIT

DWORD

Value with the changed bit

Input

X

DWORD

Value to be manipulated

N

BYTE

Position of the bit to be changed, starting with 0

B

BOOL

Value of specified bit