Schedule (STRUCT)

 

TYPE Schedule : STRUCT

InOut:

Name

Type

Comment

usiSwitch

USINT

Number of the output; Several time periods for each output are possible. [1..32]

todFirstOn

TOD

First time from which the switch is to be switched on

todLastOn

TOD

Last time until which the switch is to be switched on

byDayFlags

DAYS

The day(s) in a week this switch is active