STATISTICS_INT (FB)

 

FUNCTION_BLOCK STATISTICS_INT

Calculates minimum, maximum, and average of an input value

The calculation is done over time and can be reset in order to start a fresh caluclation/statistic.

InOut:

Scope

Name

Type

Initial

Comment

Input

IN

INT

Input value

RESET

BOOL

TRUE: AVG set to 0, MN and MX to minimum and maximum possible integer values

Output

MN

INT

32767

Minimum value

MX

INT

-32768

Maximum value

AVG

INT

Average value