STATISTICS_REAL (FB)

 

FUNCTION_BLOCK STATISTICS_REAL

Calculates minimum, maximum, and average of an input value

The calculation is done over time and can be reset in order to begin a fresh caluclation/statistic.

InOut:

Scope

Name

Type

Initial

Comment

Input

IN

REAL

Input value

RESET

BOOL

TRUE: AVG set to 0, MN and MX to minimum and maximum possible real values

Output

MN

REAL

3.402823466E+38

Minimum value

MX

REAL

-3.402823466E+38

Maximum value

AVG

REAL

Average value