FUNCTION_BLOCK VARIANCE
Calculates the mathematical variance of a variable over time
In this case, over time means that the variance is extended for each call to the function block until a reset is done.
InOut:
Scope |
Name |
Type |
Comment |
Input |
IN |
REAL |
Input value |
RESET |
BOOL |
Reset |
|
Output |
OUT |
REAL |
Variance |