FUNCTION_BLOCK WORD_AS_BIT
Converts an input value of data type WORD into 16 outputs of data type BOOL
InOut:
|
Scope |
Name |
Type |
Comment |
|
Input |
W |
WORD |
Input value |
|
Output |
B00 |
BOOL |
Output bit 0 |
|
B01 |
BOOL |
Output bit 1 |
|
|
B02 |
BOOL |
Output bit 2 |
|
|
B03 |
BOOL |
Output bit 3 |
|
|
B04 |
BOOL |
Output bit 4 |
|
|
B05 |
BOOL |
Output bit 5 |
|
|
B06 |
BOOL |
Output bit 6 |
|
|
B07 |
BOOL |
Output bit 7 |
|
|
B08 |
BOOL |
Óutput bit 8 |
|
|
B09 |
BOOL |
Output bit 9 |
|
|
B10 |
BOOL |
Output bit 10 |
|
|
B11 |
BOOL |
Output bit 11 |
|
|
B12 |
BOOL |
Output bit 12 |
|
|
B13 |
BOOL |
Output bit 13 |
|
|
B14 |
BOOL |
Output bit 14 |
|
|
B15 |
BOOL |
Output bit 15 |