FUNCTION WORD_AS_STRING : STRING(2)
Converts one word into its ASCII string representation
Example:
Input: '16#AF'
Byte order: FALSE
->
String: 'AF'
InOut:
Scope |
Name |
Type |
Comment |
Return |
WORD_AS_STRING |
STRING(2) |
A STRING(2) representing the HEX code of the input W |
Input |
W |
WORD |
Input value |
ORDER |
BOOL |
TRUE: Swaps high and low byte |