Command 'Clear authentication data'
Function: This command opens the CODESYS dialog. In this dialog, define the caches that will be deleted.
Call: Menu bar: Project ‣ SVN .
The authentication memory contains the authentication data of all SVN repositories for which the user has selected for saving the authorization data. This memory is deleted completely by this command. |
|
Clear the shared on-disk cache. |
|
Clear the RAM cache of this instance. |
|
Note
The authentication data saved on the computer is stored in %APPDATA%\\Subversion\\auth. This memory path is also used for most other Subversion client applications (for example, TortoiseSVN and AnkhSVN). Therefore, deleting the authentication data affects these applications as well.