Command 'Commit', Command 'Commit project'
Function: This command commits changes that were made in CODESYS to the SVN repository. The Commit dialog opens for this purpose.
Call:
Context menu: SVN to commit this object exactly.
Menu bar: Project ‣ SVN ‣ Commit project to commit all changes in the project at the same time.
Requirement: At least one object was edited. The edited object is overlaid in the object tree with the
icon.
When you execute the command, the block on the objects to be committed is lifted automatically.
Commit to: <URL project/object>
|
URL in SVN repository Example: file:///D:/SVN repository/trunk/ControlABC.project |
|
|
Log message |
Comment the change in a log message. Example: Bug fix error 123 |
|
Recent Messages |
Opens the dialog Recent Messages to display the last log messages. You can click a log message to accept it. |
Changes made (double-click on object for compare, right-click on object for more operations)
|
|
List of objects that were changed and can therefore be committed. The SVN URLs mirror the hierarchy of the object in the SVN repository. The objects are highlighted in color according to the object status:
Double-click an object in order to open the compare dialog. The revision of the working copy is compared with the base revision. The compare dialog also opens when you click Compare in the context menu. Right-click an object in order to open the context menu. Note: This opens a list of objects when Commit project was clicked. For the Commit command applied to a specific object, only this object is listed (if modified) and its modified children. |
|
Object |
Example: |
|
Text status |
Object status in CODESYS
|
|
Property status |
Status of the metadata of the object
|
|
Lock |
If the object has a lock, then it is shown here the user who applied the lock. Example: b.mayer |
|
Description |
Display of the log message |
|
Select/deselect all |
|
|
Keep locks |
|
|
Keep change lists: |
|
|
Update after commit (recommended) |
See also: SVN help |
|
Button Update project |
Updates the project. Tip: Prevent conflicts by committing a previously updated project/object. |
|
OK Keyboard shortcut Ctrl+Enter Keyboard shortcut Ctrl+Enter |
Checks the working copy first. Starts the commit of changes when the working copy is current. Opens a dialog when the working copy is outdated. You can then select the following:
Note: The history of the commit is displayed in the Messages view. The messages are highlighted in color.
|
Note
Handling external objects If the external object is in the same SVN repository, then changes in this external object are listed in the commit dialog and committed together with the internal project. If an external object is in another SVN repository, then you are notified about changes in the external project and you have to commit these separately.
An external object has the externals property.
See also
SVN help: http://svnbook.red-bean.com/en/1.7/svn.basic.in-action.html#svn.basic.in-action.mixedrevs)
Context menu (right-click on object)
|
|
Opens the compare dialog to compare the working copy with the top-level revision. |
|
|
Opens the compare dialog to compare the working copy with the HEAD revision. |
|
|
The list entries are highlighted in color according to the object status:
|
|
|
Discards your changes to the working copy. Then the object corresponds to the revision in the SVN repository. |
|
|
Shows the version history of the selected object. |
|
Properties |
Opens the SVN Properties dialog. The properties are displayed there and you can edit them. |
|
Move to change list |
Note: This command has not been implemented yet. |