Command 'SVN Repository Browser'
Function: This command opens the SVN repository browser. The contents of an SVN repository is shown in a tree structure here. You can search through the repository in the browser.
Call: Menu bar: Project ‣ SVN .
Depending on the selected object, the following commands are available in the context menu:
Show log
Checkout
Create folder
Copy to
Rename
Delete
Double-clicking the object with the right mouse button opens the log dialog.
Dialog 'SVN Repository Browser'
|
URL |
URL in SVN repository Example: https://svnserver/repository/trunk/ControlABC.project Tip: As soon as a valid SVN repository is specified, you can browse and select a specific project by means of the adjacent button. |
|
|
Opens the dialog Select revision. The button is labeled with the currently selected revision:
Note: The dialog provides the same options as the Revision group. |
|
|
Updates the browser view by rescanning the SVN repository. |
|
|
Navigates the URL address up by one folder. |
|
Left area |
Directory tree in the SVN repository. Project nodes are shown in bold.
|
|
Right area |
List of objects of the selected directory |
|
Close |
Closes the dialog |
See also